Welcome to EasySize (Release 1.10) for Windows
            ----------------------------------------------

  This README file contains important information about EasySize 1.10.



TABLE OF CONTENTS
-----------------
1.  Latest Update Info
2.  Installation
3.  System Requirements
4.  How To Use EasySize



 1. LATEST UPDATE INFORMATION
-----------------------------

Version

1.10 of 1/19/96

  All basic functionality complete
  Support for Graphing, Printing and Help Available
  Warning:  If the printing process is interrupted while printing a graph, 
the EasySize software may generate a general protection fault.  
To avoid this problem allow at least 5 seconds after printing a graph before 
continuing with the application.  This will be corrected in the next version.


 2. INSTALLATION
----------------

  You SHOULD use the SETUP.EXE program to install EasySize 1.10.

  To start the installation, run Windows in 386 Enhanced Mode,
  Insert the EasySize Setup/Program Disk in your Floppy Drive.
  Select File, Run from the Program Manager and type the following:

  A:SETUP.EXE<CR> ( use B: if installing from the B Drive )

  Follow the instructions given during the Setup of EasySize.


 3. SYSTEM REQUIREMENTS
-----------------------

  EasySize for Windows has the following requirements:

   - Microsoft Windows 3.1 or 3.11

   - 386DX or higher processor

   - 4 MB of memory

   - VGA or higher resolution graphics card

   - Mouse or compatible pointing device

   - 3.5 inch High Density (1.44 MB) diskette drive


 4. HOW TO USE EASYSIZE
-----------------------

  For a complete guide to using EasySize read the Getting Started section 
  in the on-line help.